A layperson’s guide to the array of desktop and mobile communication devices
Remember when a telephone sat on the desk, didn’t light up, didn’t get carried around, and certainly didn’t talk to the PC sitting right beside it? If you’re younger than 50, you might not. In mainstream business environments, digital telephony has been around since the 1980s, mobile workplace phones since the early ‘90s, and IP communications since the mid ‘90s. It has been a long time since the basic telephone and its cousin the fax machine were the primary means of connecting in the workplace.
Today business users have an impressive range of choice in phones. In fact, telephones are now so versatile, diverse and smart that they are often called endpoints. (They don’t like to be mistaken for those soulless, legacy devices that couldn’t do much more than transmit the human voice.)
Facing a new wealth of options in endpoints, how do you make the right choice for yourself? For employees throughout the office? For remote or traveling employees? Here’s a quick look at the first steps to narrowing down the choices.
To what type of business communications system will the endpoints connect?
- For a digital PBX, you’ll need digital endpoints, such as Toshiba 5000-Series digital telephones.
- For a converged system (one that supports digital or IP communications), such as a Toshiba Strata® CIX™ system, you can choose digital or IP endpoints. Analog telephones can be used for backup, ready to connect directly to analog trunks if the IP-PBX or IP network connection is unavailable.
- For a pure IP system, such as a Toshiba IPedge system, you would use IP endpoints, such as Toshiba 5000-Series IP Telephones.
Where will the endpoints be used?
If the user stays more or less at a desk – whether in a local, remote or home office…
A desktop phone with microphone and speaker (with mute options, headset interface and programmable feature buttons) is the logical choice.
If the user needs to roam around the building…
Choose a wireless handset or mobile phone that uses your wireless LAN or wireless base stations to connect into the central communications system, such as Toshiba IP4000 wireless mobility phones.
If the user travels to other locations outside your company’s phone or data networks…
Choose either: (A) a softphone client (software that empowers a PC to perform the features of a desktop phone), or (B) a network option that enables your smartphone to function as a PBX extension via the office wireless LAN while in the office and via a cellular network out of the office.
Having narrowed down the choice to digital or IP, desktop or mobile, you still have a wide range of choice in features and functionality, to find just the right model at the right price point for each user/role in the organization.